Product added to cart

Edmund Optics®

知識中心

 由我們 240 多位全球工程師創建且經過驗證的可信任技術資源庫。

Filter
Search Results for: Specialty Mirrors | 特殊平面反射鏡 (150)

桿式反射鏡

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

現在查看 添加內容至保存

高反射率反射鏡適合雷射應用

The industry standard method for quantifying reflectivity does not tell the whole story

現在查看 添加內容至保存

使用高色散超快反射鏡提供色散補償

Learn how Highly-Dispersive Mirrors compensate for dispersion and compress pulse duration in ultrafast laser systems, which is critical for maximizing performance.

現在查看 添加內容至保存

超快高色散反射鏡

Pulse Compression and Dispersion Compensation for Ultrafast Lasers

現在查看 添加內容至保存

半導體超級反射鏡

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

現在查看 添加內容至保存

E 系列動態光學反射鏡調整組件

E-Series Kinematic Optical Mounts provide high value and essential features for applications including lab use, prototyping, and system integration

現在查看 添加內容至保存

Schwarz Mirrors

Schwarz Mirrors eliminate stray light using black, engineered fused silica substrates that maintain desired characteristics while absorbing unwanted light.

現在查看 添加內容至保存

適用於雷射應用的反射式光學產品

Beam Conditioning Optics for UV, IR, and Broadband Lasers

現在查看 添加內容至保存

非球面透鏡的製造方式

Edmund Optics® manufactures thousands of precision aspheric lenses per month in our asphere manufacturing cell that operates 24 hours a day.

現在查看 添加內容至保存

全面採用非球面透鏡

Time to Replace Spherical Elements with Aspheric Lenses

現在查看 添加內容至保存

下一代球面透鏡

Traditional spherical lenses are evolving due to the increasing demands of applications. Learn about the future of spherical lenses at Edmund Optics.

現在查看 添加內容至保存

高反射率鍍膜

高反射率 (HR) 鍍膜應用於光學元件,以最大限度地減少反射雷射和其他光源時的損失。

現在查看 添加內容至保存

愛特蒙特光學的度量技術:將測量作為製造的關鍵要素

Learn about the metrology that Edmund Optics® uses to guarantee the quality of all optical components and assemblies.

現在查看 添加內容至保存

盡可能減少超快系統的熱透鏡效應

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

現在查看 添加內容至保存

電影鏡頭、串流時代及非球面透鏡

Cinema lenses designed to create content tailored for online streaming utilize aspheres to shoot with a shallow depth of field while maintaining quality.

現在查看 添加內容至保存

抗反射 (AR) 鍍膜

抗反射 (AR) 鍍膜應用於光學元件,以提高吞吐量並減少背反射造成的傷害。

現在查看 添加內容至保存

雷射擴束鏡

雷射擴束鏡對於降低功率密度、最小化遠距離光束直徑以及最小化聚焦雷射光斑尺寸至關重要。

現在查看 添加內容至保存

反射鏡金屬鍍膜

Want to learn more about metallic mirror coatings? Find information about standard and custom metallic mirror coatings that are available at Edmund Optics.

現在查看 添加內容至保存

為什麼要選擇消色差柱面鏡?

Debating whether or not to use a traditional cylinder lens or an achromatic cylinder lens? Discover the benefits of achromatic cylinder lenses at Edmund Optics.

現在查看 添加內容至保存

紫外雷射

A new generation of small, cost-effective, CW ultraviolet (UV) lasers allows more applications to move to UV wavelengths for increased power and precision.

現在查看 添加內容至保存

鑽石車削離軸拋物面反射鏡的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

現在查看 添加內容至保存

液態透鏡特性、應用以及技術

液體鏡頭具有許多特點,體積小,可以快速調整焦距以適應位於不同工作距離的物體。在愛特蒙特光學了解更多。

現在查看 添加內容至保存

2µm 雷射

The unique absorption properties of 2µm lasers allow them to create small and precise cuts for medical and materials processing applications

現在查看 添加內容至保存

非球面透鏡不規則 度及 Strehl 比

光學系統的 Strehl 比是其實際性能與其衍射極限性能的比較。

現在查看 添加內容至保存

未來的顯微鏡物鏡

Advances in Microscopy Tackle the Challenges of the Future

現在查看 添加內容至保存

單點鑽石車削:愛特蒙特光學依圖建置的製造

Edmund Optics utilizes Diamond Turning to produce a wide range of high precision optical components.

現在查看 添加內容至保存

調制轉換函數在鏡頭設計中的像差平衡

您是否有多個涉及使用鏡頭的項目?在愛特蒙特光學了解可用於多種用途的不同鏡頭。

現在查看 添加內容至保存

愛特蒙特光學遍佈全球的製造工廠

Edmund Optics® (EO) manufactures millions of precision optical components and subassemblies every year in our 5 global manufacturing facilities.

現在查看 添加內容至保存

用於成像的液態鏡頭

Quickly Autofocus and Overcome Depth of Field Limitations

現在查看 添加內容至保存

雷射光束整型概觀

了解如何瀏覽用於塑造雷射光束的輻照度輪廓和相位的許多可用選項,以最大限度地提高雷射系統的性能。

現在查看 添加內容至保存
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin